Part Number: MSP430FR2311
Hi TI Team,
I am working on a project in which I would like to use a MSP430FR2311 microcontroller, that acts as a UART to I²C Bridge and as Port Expander at the same time.
I found many examples of firmware ready to use it. One of these examples is used as a UARTto I²C Bridge, but there is no possibility to control an external gpio. I would like to be able to control GPIO by sending commands through the UART writed to the internal registers of the MSP430. Do you have firmware in which these two functions are implemented?
Best Regards,
Piotr