This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2419: Flash in linux without CCS

Part Number: MSP430F2419

Hello TI,

I want to flash my msp430f2419 using the FET debugger. Whenever I use an application or program that uses MSP430_GetNumberOfUsbIfs I get Segmentation fault (core dumped). 

Command: mspdebug tilib

root@w03wibenp1:~# mspdebug tilib
MSPDebug version 0.22 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2013 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

MSP430_GetNumberOfUsbIfs
Segmentation fault (core dumped)

root@w03wibenp1:~/ti/MSPFlasher_1.3.20# file libmsp430.so

libmsp430.so: ELF 64-bit LSB shared object, x86-64, version 1 (SYSV), dynamically linked, BuildID[sha1]=03893b73ce39c27f450109fe574f3b64d2e1ff75, stripped

root@w03wibenp1:~/ti/MSPFlasher_1.3.20# uname -a
Linux w03wibenp1 4.4.0-19041-Microsoft #3636-Microsoft Thu Oct 19 17:41:00 PST 2023 x86_64 x86_64 x86_64 GNU/Linux

Any help is appreciated! 

Best Regards

Wissem 

**Attention** This is a public forum