This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5308: DCO Clock accuracy

Genius 3215 points

Part Number: MSP430F5308

Hi,All

(For a board ambient temperature of 22.2°C, humidity of 42%, DCO 25Mhz)
What is the clock accuracy?

Please let me know the clock accuracy under my conditions, not under the conditions of the datasheet.

MSP430F5310, MSP430F530x Mixed-Signal Microcontrollers datasheet (Rev. G) (ti.com) [5.18]

Best Regards,
Ito

  • Hi ito-kaz,

    If the specific information is not shown in the datasheet then it is most likely not available (not tested).  For this request, there is no additional test data available for this specific humidity, temperature and frequency.

**Attention** This is a public forum