Part Number: MSPCAPTDSNCTR
The previous thread with this title is now 2 years old. There it was mentioned, that the problem with the java-path will be fixed in Q1 2022.
e2e.ti.com/.../mspcaptdsnctr-java-runtime-issues-user-interface-does-not-work-on-windows-11
I just downloaded the current version - it is still 1.83.00.08, which of course still doesn't work. Of course the workaround works perfectly. But there is another annoying bug: The application doesn't work with the current Java-versions. I tried the newest JDK 21.0.2, then trying older versions, ending up at JDK 11.0.21, which works. The newer versions just throw an exception and the GUI just creates strange effects, not working at all. Did I just catch the wrong path for download or is there any intention to update the application to fix these bugs?
Regards,
Klaus