This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: MSP430-FR6047 I have a question about i2c port connection.

Part Number: MSP430FR6047
Other Parts Discussed in Thread: EVM430-FR6047,

Hello

I have a question about i2c port connection.

I understand that in order to use USS from TI, I only need to connect the I2C IRQ/SDA/SCL pin of the EVM430-FR6047 and it will work.

Currently, our board uses the I2C Pin to connect to COMM_IRQ / COMM_SDA / COMM_SCL of EVM 430-FR6047 as shown below.

And, if you look at the USS Connection, only waiting for device appears as shown below, and the normal Connected message does not appear.

EVM LED

LED1 - off

LED2 - off

LED3 - RED

D201 - GREEN

D202 - GREEN Blink ( in below status)

D203 - off

POW_SEL - ezFET (mid position)

How can I establish a normal connection to USS?

For reference, on the MSP430FR6047 board under development, I connected the MSP430FR6047 chip to COMM_IRQ/COMM_SDA/COMM_SCL as shown below.

And, both the custom board and the EVM are operating with the FW raised.

**Attention** This is a public forum