This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR5994: MSP-EXP430FR5994 Launchpad Kit

Part Number: MSP-EXP430FR5994


I am trying to use MSP_EXP430FR5994 Launchpad kit for SD read/write operation. Now the kit is not detected by the PC, no communication ports are available(it is showing that the USB device not recognized). The red led(LED101) is glowing once USB cable is connected to the PC and the green led(LED102) is blinking in irregular interval. i have reinstalled the FET-Z driver also. Please help me solve the problem.

**Attention** This is a public forum