Part Number: MSP430F2132
Hello
Do you need external crystal for i2c 100kHz or 400kHz when using the eUSCI in slave mode
Thanks in advance
Stéphane
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F2132
Hello
Do you need external crystal for i2c 100kHz or 400kHz when using the eUSCI in slave mode
Thanks in advance
Stéphane
Short answer: No, the master provides the clocking. [Ref User Guide (SLAU144K) Sec 17.3.5]
You may want to run the CPU at a reasonable speed (1MHz?) to assure responsiveness, but you don't need the clock accuracy of a crystal, the DCO will be fine.
Dear
That is clear.
I try to find " MSP430F21x2 Code Examples (Rev. C): www.ti.com/.../slac163c " but the link is wrong
What is now the link ?
I searched ti.com for "slac163" and ended up here:
https://www.ti.com/tool/download/SLAC163
These are also available in Resource Explorer here:
https://dev.ti.com/tirex/explore/node?node=A__AA9hfDmh39HASB2FIu6KKQ__msp430ware__IOGqZri__LATEST
I just past and copy one of the examples in iRA 8.00 but i do not receive
data
What happens
#include <msp430.h>
;-------------------------------------------------------------------------------
RSEG CSTACK ; Define stack segment
;-------------------------------------------------------------------------------
RSEG DATA16_N ; RAM
RxData DS 128 ; Allocate 128 byte of RAM
;-------------------------------------------------------------------------------
RSEG CODE ; Assemble to Flash memory
;-------------------------------------------------------------------------------
RESET mov.w #SFE(CSTACK),SP ; Initialize stackpointer
// dint
StopWDT mov.w #WDTPW+WDTHOLD,&WDTCTL ; Stop WDT
CheckCal cmp.b #0FFh,&CALBC1_16MHZ ; Calibration constants erased?
jeq Trap
cmp.b #0FFh,&CALDCO_16MHZ
jne Load
Trap jmp $ ; Trap CPU!!
Load mov.b &CALBC1_16MHZ,&BCSCTL1 ; Set DCO to 16MHz
mov.b &CALDCO_16MHZ,&DCOCTL
SetupP3 bis.b #06h,&P3SEL ; Assign I2C pins to USCI_B0
SetupUCB0 bis.b #UCSWRST,&UCB0CTL1 ; Enable SW reset
mov.b #UCMODE_3+UCSYNC,&UCB0CTL0
; I2C Slave, synchronous mode
mov.w #010h,&UCB0I2COA ; Own Address is 010h
bic.b #UCSWRST,&UCB0CTL1 ; Clear SW reset, resume operation
bis.b #UCSTPIE+UCSTTIE,&UCB0I2CIE
; Enable STT and STP interrupt
// eint
bis.b #UCB0RXIE,&IE2 ; Enable RX interrupt
Main mov.w #RxData,R5 ; Start of RX buffer
clr.w R6 ; Clear RX byte count
// bis.b #LPM0+GIE,SR ; Enter LPM0, enable interrupts
; Remain in LPM0 until master
; finishes TX
nop ; Set breakpoint >>here<< and
; read out the RxData buffer
jmp Main ; Repeat
;-------------------------------------------------------------------------------
; The USCI_B0 data ISR is used to move received data from the I2C master
; to the MSP430 memory.
;-------------------------------------------------------------------------------
USCIAB0TX_ISR; USCI_B0 Data ISR
;-------------------------------------------------------------------------------
mov.b &UCB0RXBUF,0(R5) ; Move RX data to address R5
inc.w R5 ; Increment address pointer
inc.w R6 ; Increment RX byte count
reti
;-------------------------------------------------------------------------------
; The USCI_B0 state ISR is used to wake up the CPU from LPM0 in order to
; process the received data in the main program. LPM0 is only exit in case
; of a (re-)start or stop condition when actual data was received.
;-------------------------------------------------------------------------------
USCIAB0RX_ISR; USCI_B0 State ISR
;-------------------------------------------------------------------------------
bic.b #UCSTPIFG+UCSTTIFG,&UCB0STAT
; Clear interrupt flags
tst.w R6 ; Check RX byte counter
jz USCIAB0RX_ISR_1 ; Jump if nothing was received
// bic.w #LPM0,0(SP) ; Clear LPM0
USCIAB0RX_ISR_1
reti
;-------------------------------------------------------------------------------
COMMON INTVEC ; Interrupt Vectors
;-------------------------------------------------------------------------------
ORG USCIAB0TX_VECTOR ; USCI_B0 I2C Data Int Vector
DW USCIAB0TX_ISR
ORG USCIAB0RX_VECTOR ; USCI_B0 I2C Sate Int Vector
DW USCIAB0RX_ISR
ORG RESET_VECTOR ; POR, ext. Reset, Watchdog
DW RESET
END
How do you tell that it isn't receiving data? When you pause in the debugger, where is it executing?
-----------------
I don't have IAR, but it looks as though you modified these two lines:
> // bis.b #LPM0+GIE,SR ; Enter LPM0, enable interrupts
> // bic.w #LPM0,0(SP) ; Clear LPM0
Removing them would prevent receiving data. I suggest you put these lines back.
Dear
i try to detect a repeated start as i2c slave.
do you have an explantion of examples , how to proceed ?
Hi, Stephane
During transmission, if a start interrupt is triggered without a stop interrupt, that is a repeated start.
Regards,
Helic
Hi, Stephane
I didn't find demo code of this.
Just set some kind of I2C_Status_flag variables in I2C interrupt is OK.
Such as:
void I2C_Start_interrupt_Handler(){
if(I2C_STATUS_RX_STARTED){
I2C_STATUS_RX_REPEATED_STARTED = true;
}
else{
I2C_STATUS_RX_STARTED = true;
}
}
void I2C_Stop_interrupt_Handler(){
I2C_STATUS_RX_REPEATED_STARTED = false;
I2C_STATUS_RX_STARTED = false;
I2C_STATUS_RX_STOP = true;
}
Regards,
Helic
**Attention** This is a public forum