Other Parts Discussed in Thread: MSP430G2211
Hi,
I am doing on of my project with msp430g2211 controller.the controller have only one port.if i am using 4 bit mode communication means
P1.4 ->D4
P1.5 ->D5
P1.6 ->D6
P1.7 ->D7
P1.0 ->E
P1.1 ->RS
The remaining Pins 1.2 & 1.3 i used for other inputs like switch and other.if i am using like this whether it will cause any problem?will i use the remaining 2 pins for others?
Thanks in advance.
Joseph.D