This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A: GPIO Interrupt flag set

Part Number: MSP430F5438A


Hi,

1.What are the factors for setting the interrupt flag?

2. I'm trying to configure the GPIO interrupt to only happen from high to low [Falling Edge], but the flag is set to 1 at the time the pin goes from low to high. What causes this problem?

My configuration is mentioned below.

P1DIR &= ~BIT2; 
P1REN |= BIT2;
P1IE |= BIT2;
P1IES |= BIT2;
P1IFG &= ~BIT2;

Thank You...!

**Attention** This is a public forum