This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0C1104: Cannot connect debugger after setting watchdog

Part Number: LP-MSPM0C1104

Hi please help,

I configured a watchdog of period 15.63ms and PDBGCTL.FREE set to 1.

Now I cannot reprogram/flash the chip.

I am using the debugger of the launchpad Rev E3.

The error is: "Error connecting to the target: (Error -2063 @ 0x0) Unable to reset device. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.6.0.00029)".

Thanks in advance.

**Attention** This is a public forum