This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: Incorrect standard deviation in USS Design Center GUI

Part Number: EVM430-FR6047


I'm using EVM430-FR6047 with USS Design Center and MSP430FR6047EVM_USS_Demo project.

Design Center GUI and demo project versions are 02_40_00_00.

In Design Center User's Guide, we can custom the debug waveform,

so I check the Debug waveform with hard coded float value. (1.0 in plot 2 and 4.0 in plot 3)

Graph looks good, but standard deviation is not zero even thought all of the values are the same.

It looks like standard deviation is the root of Mean value.

Isn't standard deviation value zero when all of the values are the same?

**Attention** This is a public forum