Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
from default value to for example 48MHz or 32MHz or 24MHz (benchmark evaluation)
thx
LG
Vincenzo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
from default value to for example 48MHz or 32MHz or 24MHz (benchmark evaluation)
thx
LG
Vincenzo
Hi Vincenzo,
Are you using SysConfig? The 32MHz clock is just the base SYSOSC frequency. That should be the default in most examples.
For 48MHz and 24MHz you should use the SYSPLL. This is very easy to configure in clock tree. To do that you first you need to ensure that clock tree is enabled within the sysconfig SYSCTL module.

Then within clock tree you can set the PDIV and QDIV and other divider values such that MCLK is the frequency you want.

Best Regards,
Brandon Fisher
hi Brandon,
thanks a lot.
The idea for the long run is to have an header where to change some variables and set "on the fly" the main clock frequency.
I wasn't able to find anything like that. May you help me out w/ that?
thx again
LG
Vincenoz
**Attention** This is a public forum