Part Number: MSP430F6779A
Is there specification about VLO Clock start-up time?
After reset, How long do we have to wait for the VLO clock to stabilize?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F6779A
Is there specification about VLO Clock start-up time?
After reset, How long do we have to wait for the VLO clock to stabilize?

Hi TinK,
I also do not find the start-up time for VLO clock.
Actuallt after reset, you should wait for internal oscillator ready and then run boot code and application code. I think it not necessary for focus on VLO start up time.
B.R.
Sal
Hi Sal,
Thank for information.
Now i have some problem related to the Auxiliary module that use VLOCLK same as issues below.
e2e.ti.com/.../msp430f6779a-auxxsw-not-operation

AUX2SW, AUX1SW and AUX0SW are always zero after the code "AUXCTL0 = AUXKEY"(tests using a DVCC supply on 3.3 and then off 0 V, problems occurring in approximately 0.1 % of the total number of trials).
Is the VLO clock always ready to work after released from the MCU reset state?
Do you think possible to cause from VLO clock not work in short time from reset? (so may need to add delay time before setting the AUX module)
Hi Tink,
Is the VLO clock always ready to work after released from the MCU reset state?
From my perspective, I think it is ready.
How about the DVCC supply volateg? I actually find a ERRATA which descibes a bug:

B.R.
Sal
**Attention** This is a public forum