Other Parts Discussed in Thread: MSP430FR2476, LP-MSPM0L1306
Hi team,
- For LP-MSP430FR2476, "P4.0" and "P2.3" are used for Input, and external pull-up resistors R9 and R10 are implemented.
But if the internal pull-up resistors are enabled, is it correct that R9 and R10 are not necessary?.
Or do the "P4.0" and "P2.3" have no internal pull-up resistors? -
For MSP430FR2476, Are there any pins where customers cannot set the internal pull-up resistor in the "input" setting of the GPIO?
-
For MSP430FR2476, Customer would like to set the GPIO Output setting to "High-Level" (about 3.3[V] output when on) and measure the "output" value with an oscilloscope.
Should they implement limiting resistors?
If yes, how many Ω resistors should you put in if you want to implement it?
Thank you in advance.
Best regards,
Kenley