hi there,
i am using the template code FR6043_USSSWLib_template_example. I want to use the UART for debug, APPLICATION_ENABLE_UART_DEBUG. Where should i connect my USB2UART Tx Rx cable, on the EVM.
what UART/pin is being used on the MSP.
thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi there,
i am using the template code FR6043_USSSWLib_template_example. I want to use the UART for debug, APPLICATION_ENABLE_UART_DEBUG. Where should i connect my USB2UART Tx Rx cable, on the EVM.
what UART/pin is being used on the MSP.
thanks,
Hi
I just searched in the template examples and couldn't find APPLICATION_ENABLE_UART_DEBUG. There is no UART communication function in this project, FR6043_USSSWLib_template_example. Secondly, you can add UART functionality yourself, using the backchannel UART interface implemented on the EVM.
Please refer to the MSP430FR6043-based ultrasonic gas flow meter quick start guide (Rev. B)
the schematics for the EVM at https://www.ti.com/lit/pdf/tidrys5
Thanks!
**Attention** This is a public forum