Part Number: MSP430FR6989
Team,
The datasheet is only showing the digital input threshold levels for 2.2 V and 3.0 V supply. How are these levels if VCC=2.8 V?

Thanks,
Robert
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6989
Team,
The datasheet is only showing the digital input threshold levels for 2.2 V and 3.0 V supply. How are these levels if VCC=2.8 V?

Thanks,
Robert
Hi Robert,
The threshold values tend to be a ratio of your VCC levels. Here are my approximations for 2.8V. (A curve can be created if you need a higher accuracy for the min and max thresholds)
| Positive Input Threshold | |||||
| VCC | Min | Min Ratio | Max | Max Ratio | |
| 2.2 | 1.2 | 0.545 | 1.65 | 0.75 | |
| 3 | 1.65 | 0.55 | 2.25 | 0.75 | |
| Approximation | 2.8 | ~1.53 | 2.1 | ||
| Negative Input Threshold | |||||
| VCC | Min | Min Ratio | Max | Max Ratio | |
| 2.2 | 0.55 | 0.25 | 1 | 0.4545 | |
| 3 | 0.75 | 0.25 | 1.35 | 0.45 | |
| 2.8 | 0.7 | ~1.26 | |||
Regards.
Luke
**Attention** This is a public forum