Part Number: LP-MSPM0C1104
Other Parts Discussed in Thread: SYSCONFIG, MSPM0C1104
Hello everyone,
I am new with this EVB and MCU. I want to create a systicks running a 100us and trigger systick interrupt handler.
Here is the problem.
I can enable systicks and enable SysTick Interrupt.
However, within the SYSTICK interrupt vector service program, I have been unable to observe the SYSTICK interrupt occurring.
I also not found this example in the SDK, how should I activate it ?
Here is code:
uint16_t systick_count;
SYSCONFIG_WEAK void SYSCFG_DL_init(void)
{
SYSCFG_DL_initPower();
SYSCFG_DL_GPIO_init();
SYSCFG_DL_SYSCTL_init();
DL_SYSTICK_config(2400); //1/24MHz = 41.66ns, 41.66ns x 2400 = 100us
}
void SysTick_Handler(void)
{
systick_count++;
}
Can someone help answer this?
Thanks!