Part Number: MSP-EXP430FR2311
Other Parts Discussed in Thread: LM3648, , USB2ANY
I wired MSP-EXP430FR2311 the same way as SLAA908A instructed. Download the firmware image file from SLAA908A to MSP-EXP430FR2311 through CCS. When I connect MSP-EXP430FR2311, two UART ports are populated: MSP application UART1 and MSP debug Interface. I tried to read register of LM3648 through UART terminal. UART port "MSP application UART1" is configured to be baudrate 115200, 8 bit data , no parity, 1 stop bit, no flow control. Send hex number sequence "0x53(start) 0xC6(device address+write) 0x0C(register address) 0xC7(device address+read) 0x50(stop)" to LM3648 to read ID register 0x0C. No data is returned from LM3648.
I have confirmed LM3648 works well by using USB2ANY. May I know what could be wrong with implementing SLAA908A on MSP-EXP430FR2311?
Thanks in advance.