Which reset (PUC/POR/BOR) disables GIE?
6.3.3 Status Register (SR)
GIE General interrupt enable. When this bit is set, it enables maskable interrupts. When it is reset, all maskable interrupts
are disabled.
Which reset (PUC/POR/BOR) disables GIE?
6.3.3 Status Register (SR)
GIE General interrupt enable. When this bit is set, it enables maskable interrupts. When it is reset, all maskable interrupts
are disabled.
Hi
I test enable the GIE and then make watchdog timout.
The result the GIE is reset to 0 with the reset cause (SYSRSTIV) 16h = WDT time out (PUC).
Does it mean specific timing that the GIE is reset by PUC?
Hi TinK,
This should be reset during PUC actually.
The User's Guide covers the syntax here.
Best Regards,
Brandon Fisher
**Attention** This is a public forum