Other Parts Discussed in Thread: TPS23881
Hi,
We found an POE issue from the customer. Please help check the following description and help advise next action. Additionally, please let us know if you submit a ticket to TI E2E forum. Thanks.
Our system include MSP430F5234IRGZR with 12 PSE controllers(TPS23881). In our system, we specified two POE budget based on PSU status. When 2 PSUs are plugged, the total POE budget can reach 1800W. When only one PSU is available, the POE budget falls to 780W. Additionally, all ports are set to the same priority. I’ve attached the configuration file for your reference.
We aimed to observe the system would be stable after unplugging one PSU. We did two experiments below and found two different results. However, we found an issue in Test Case#2. This issue is more likely to reproduce with 90W per port and total consumption over 1565+W. We also tried two types of load cases: 48 ports with 30W and 25 ports with 60W. In both cases, we could not reproduce this issue.
Test configuration
- 48Port PoE Switch
- Total two PSUs present in the system. Each PSU is available to supply 1200W
- POE
- MCU: MSP430F5234IRGZR
- PSE: 12x TPS23881
- Poe Firmware Version:1.54.23.224
- 90W per port, the maximum system POE load is limited to 1800W)
- All ports are set to high-priority
Test Case#1
Test procedure:
- When the system is with 2 PSUs present, the total POE is around 1400-1500W. We tried to load two cases: 48 ports with 30W and 25 ports with 60W.
- Unplug PSU2, the system turn off partial POE ports to limit the total POE within 780W.
- Re-plug PSU2. The total POE load are back to 1400W-1500W in 1 minutes.
Test Case#2
Test procedure:
- When the system is with 2 PSUs present, the total POE is around 1500W. The maximum port load is 90-92W
- Unplug PSU2, the system did not turn off partial POE load as Test Case#1. Therefore, we observed the system off because the PSU1 is OCP.
We found an issue when most of ports are with 90W POE load.
Interface Status State Max-Power(W) Power-consumption(W) Priority Class Error
------------------------------------------------------------------------------------------------------------
port1 Enabled Delivering Power 24.46 91.40 Low 8
port2 Enabled Delivering Power 24.46 90.90 Low 8
port3 Enabled Delivering Power 24.46 90.50 Low 8
port4 Enabled Delivering Power 24.46 91.20 Low 8
port5 Enabled Delivering Power 24.46 90.90 Low 8
port6 Enabled Delivering Power 24.46 90.80 Low 8
port7 Enabled Delivering Power 24.46 90.80 Low 8
port8 Enabled Delivering Power 24.46 91.10 Low 8
port9 Enabled Delivering Power 24.46 92.40 Low 8
port10 Enabled Delivering Power 24.46 92.00 Low 8
port11 Enabled Delivering Power 24.46 92.10 Low 8
port12 Enabled Delivering Power 24.46 92.60 Low 8
port13 Enabled Delivering Power 24.46 92.90 Low 8
port14 Enabled Delivering Power 24.46 92.20 Low 8
port15 Enabled Delivering Power 24.46 92.50 Low 8
port16 Enabled Delivering Power 24.46 92.60 Low 8
port17 Enabled Delivering Power 60.00 40.70 Low 5
port18 Enabled Delivering Power 60.00 56.60 Low 6
Bryant