Part Number: MSP430FR2433
Hi to All,
What is the absolute error and accuracy of the Temperature reading when using the internal temperature sensor (in a MSP430FR2433)?
It based on the ADC specific channel included in the MSP430FR2433,
If it is acquired through a sequence of readings exploiting the multiply channel sample method, that automatically switches the analogue mux, then can be affecting this the temperature readings by the signal present on the other analogue channels?
We didn't find out any accuracy information on the data sheet for this temperature sensor, except the registers to read and the formula to apply to convert the ADC reading into a °C or °F.
We missed something published by TI?
Based on our first evaluation (with about 10 samples) we found errors between -3°C to +3°C from the ambient temperature (22°C), with an overall chip consumption below 2mW in average (measured by the Energy Trace Technology).
Is it conforming the Chip specification?
Thanks
Best Regards