Part Number: MSP430FR6047
What is the maximum frequency that MSP430FR6047 can generate using the 16MHz crystal? I know it can go a bit above 1 MHz, but I am wondering if it can go up to 8 MHz? For frequencies higher than 8 MHz shall I use DCO?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR6047
What is the maximum frequency that MSP430FR6047 can generate using the 16MHz crystal? I know it can go a bit above 1 MHz, but I am wondering if it can go up to 8 MHz? For frequencies higher than 8 MHz shall I use DCO?
Hi Aiden,
For the timer operation, when you want to output higher frequency, which means that you will get lower accuracy of the PWM adjustment.
According to datasheet:

Yes you can set a timer to output 8MHz PWM with the clock 16MHz from SMCLK/ACLK, then the output PWM can be only set as 0%/50%/100% duty cycle.
As for USS module, it can use external 4MHz or 8MHz OSC:

B.R.
Sal
**Attention** This is a public forum