This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6047: EVM430-FR6047 PC connect issue

Part Number: EVM430-FR6047
Other Parts Discussed in Thread: UNIFLASH

Hi,

I use the EVM430-FR6047 connenct to the PC, but it shows there are two port connected(show below), the location info is the same.  I have trasfer to another PC, still two ports.

In this situaiton, I use the UNIFLASH and CCS, it work normal, can download the codes, but when I connect to the USS, it can't be connected and show the notice(see below). 

Another info is I have put the EVM430-FR6047  connected to the USB docking station. Before that, I was connect the PC directly and the USS was working well.

Now, what should I do?

**Attention** This is a public forum