Part Number: MSP430FR2033
Hi team,
How long does it take to read 96 bytes of data from FRAM to RAM?
The core frequency is 1 MHz.
The program is on FRAM.
96cycle?
Best regards,
Goto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2033
Hi team,
How long does it take to read 96 bytes of data from FRAM to RAM?
The core frequency is 1 MHz.
The program is on FRAM.
96cycle?
Best regards,
Goto
If you want to copy data from FRAM to RAM, it will take more than one cycle per byte.
For example, reading with mov.w @R13+, R15 will take 2 cycles, and store mov.w R15, 0(R14) will take 3 cycles, and one cycle for R14 increment, total 6 cycles per word.
This is without loop test for R13 (or R14) border for each iteration.
Hey Goto,
Zrno has a very detailed answer. If you write the code in code composer, you can also look at the disassembly to see the assembly instructions the c-compiler used and try and count the cycles like Zrno did from there.
Thanks,
JD
**Attention** This is a public forum