This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: Averaging methods used by USS design Center

Part Number: MSP430FR6043


Tool/software:

Hello?!

I'm using the MSP430FR6043 as a Water Flow meter to confirm if water is flowing.

I'm not measure the speed of flow.

Since it's for a simple purpose of determining water flow, I'm using an 8mm diameter tube that doesn't meet the recommended diameter.

Applying a moving average to delta TOF enables us to determine the presence of water flow.

but It seems that the performance of the moving average code I created is not on par with the average performance seen at the USS Design Center.

so I just wondering about the averaging method used by the USS Design Center.

It's about the graph that appears when you check 'Plot Delta TOF mean'.

**Attention** This is a public forum