This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Due to increasing code complexity we are planning to change the existing MSP430F413 (8K flash, 256 bytes RAM) on our board with MSP430F415( 16K flash, 512 bytes RAM).
we do not intend to have any hardware (I/O pins,peripheral configuration etc ) changes.
Are there any known issues in migrating from MSP430F413 to MSP430F415 (when there are NO hardware changes)
F415 has fewer bugs as compared with F413. (See the Errata.) Hopefully, that is not an issure.
**Attention** This is a public forum