http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/getting_started.page#decoder

Memory Type: Wot - no FRAM?!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
http://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/getting_started.page#decoder

Memory Type: Wot - no FRAM?!
I augmented this a little last year when trying to characterize the different chips for mspgcc support. Some extra details are in the decoding below, but in practice I think this decoding scheme no longer works: both the FRAM and BlueTooth-optimized MCU identifiers are inconsistent with it since digraphs are now used as single identifiers at the point where memory type and end-equipment optimization used to appear.
MSP 430 F G 4 6 19 S I QZW R
-+- -+- + + + + -+ + + -+- +
| | | | | | | | | | |
| | | | | | | | | | + Optional: Distribution format
| | | | | | | | | | R = Tape & Reel
| | | | | | | | | |
| | | | | | | | | +--- Package
| | | | | | | | |
| | | | | | | | +------ Optional: Temperature range (C)
| | | | | | | | I = -40 to 85
| | | | | | | | T = -40 to 105
| | | | | | | |
| | | | | | | +-------- (UNDOCUMENTED) Packaging variant MSP430x31x
| | | | | | | S = 48-pin SSOP (vs standard 56-pin SSOP)
| | | | | | |
| | | | | | +---------- Family (memory size and peripheral configuration)
| | | | | |
| | | | | +------------- Series of similar function
| | | | |
| | | | +--------------- Generation
| | | | 1 = 1xx
| | | | 2 = 2xx
| | | | 3 = 3xx
| | | | 4 = 4xx
| | | | 5 = 5xx
| | | | 6 = 6xx
| | | | 0 = Undocumented (custom chip? MSP430C091)
| | | |
| | | +----------------- Optional: End-equipment optimized
| | | G = Medical
| | | E = Energy Meter (MSP430FE423)
| | | W = Electronic Flow Meters (MSP430FW423)
| | |
| | +------------------- Memory Type
| | C = ROM
| | E = EPROM
| | F = FLASH
| | G = FLASH (Value Line device)
| | P = OTP
| | L = No non-volatile memory (MSP430L092)
| |
| +---------------------- 430 MCU Platform
|
+-------------------------- Processor Family
CC = ChipCon Radio
MSP = Mixed Signal Processor
XMS = Experimental Silicon
Non-conformant parts:
msp430bt5190 -- BT apparently denotes a part designed to work with the
CC2560 Bluetooth radio chip. This is an msp430f5438 with the BT stack
already programmed in.
Peter Bigot said:msp430bt5190 -- BT apparently denotes a part designed to work with the
CC2560 Bluetooth radio chip. This is an msp430f5438 with the BT stack
already programmed in.
Not 'programmed-in', but with a (undisclosed) hardware difference that is checked in the BT stack library and verifies that the license fee for the stack has been paid for this device. Sort of a BT 'dongle' bit somewhere.
Could well be, but the TI contact I asked last year told me "this device is identical to the F5438 just got number differently as it has the BT stack already programmed in it." so that's what I documented.
Maybe your contact used a sloppy expression.Peter Bigot said:Could well be, but the TI contact I asked last year told me "this device is identical to the F5438 just got number differently as it has the BT stack already programmed in it." so that's what I documented.
The MindTree BT stack comes as library and is included into the binary. It is not 'already programmed'. It's possible that the MSP comes preprogrammed with the demo code, but when you want to do your own applicaiton, teh BT code is erased liek any othe rapplication code and replaced by yours.
That's why people complain that for building their own projects they need to buy a full IAR license: Since the BT stack only comes as precompiled library, and is larger than the free IAR code size limit, they need to pay for a full unlimited IAR version in order to use the BT.
From information I got here in this forum (from a TI employee), it seeems that the BT library checks for an intentional hardware anomaly that separates a BT from a real 5438.
I don't know what difference this is, maybe just the part ID in the TLV structure.
Hi All,
I just wanted to point you to a new blog post that includes the most recently updated part number decoder:
Stephanie Hsu said:I just wanted to point you to a new blog post that includes the most recently updated part number decoder:
Thanks for the info.
One thing I wondered on a second look:
the 'L' marking is listed as 'non-volatile memory'. Didn't it stand for 'low voltage device'? The L092 does have volatile memory only and requires extrernal non-volatile memory for booting (FLASH won't run on such a low voltage)
Jens-Michael Gross said:One thing I wondered on a second look:
the 'L' marking is listed as 'non-volatile memory'. Didn't it stand for 'low voltage device'? The L092 does have volatile memory only and requires extrernal non-volatile memory for booting (FLASH won't run on such a low voltage)
I believe that says "no non-volatile memory".
I, in turn, noticed that the P memory type for OTP got dropped. There are a few P chips (e.g., msp430p315) that are still listed in the devices list I get from TI for msp430mcu.
On the whole, this is a great improvement and help, and I thank TI for updating it as now I don't have to maintain my hacked-up text illustration any more....
Peter
You're right, my eyes. Maybe I thought I was just squinting when reading this double-negation.Peter Bigot said:I believe that says "no non-volatile memory".
Hey, it was a nice piece of work.Peter Bigot said:I don't have to maintain my hacked-up text illustration any more..
Officially, the 3x family is discontinued. But maybe there are some special customers who still order significant amounts or have a supply contract with TI that isn't expired yet.Peter Bigot said:There are a few P chips (e.g., msp430p315) that are still listed in the devices list
Jens-Michael Gross said:Hey, it was a nice piece of work.[/quote]I don't have to maintain my hacked-up text illustration any more..Thank you.
Jens-Michael Gross said:Officially, the 3x family is discontinued. But maybe there are some special customers who still order significant amounts or have a supply contract with TI that isn't expired yet.[/quote]There are a few P chips (e.g., msp430p315) that are still listed in the devices listI don't think the details in the PN decoder should be limited to currently available chips; ideally it will cover the entire product history, so it can be used to identify the characteristics of some legacy hardware found gathering dust in a desk drawer. I would look to the decoder to answer "What does this P mean" if I encountered one of those chips in the wild. (Though it would also help if "OTP" was defined somewhere in the diagram.)
Peter
Jens-Michael Gross said:Since the key is headline memory type/device type, I think the 'low voltage' is the dominant attribute of the L devices rather than the fact that they don't have non-volatile memory (and in fact, some L devices have - just not for program execution and only for high-voltage operation, at least during boot)
Thank you for bringing this up. We originally defined "0" as the low voltage series and wanted to keep the "Memory Type" category specifically memory. However, if this causes confusion, we'd be more than willing to modify "L" to low-voltage.
Peter Bigot said:Officially, the 3x family is discontinued. But maybe there are some special customers who still order significant amounts or have a supply contract with TI that isn't expired yet.[/quote]There are a few P chips (e.g., msp430p315) that are still listed in the devices listI don't think the details in the PN decoder should be limited to currently available chips; ideally it will cover the entire product history, so it can be used to identify the characteristics of some legacy hardware found gathering dust in a desk drawer. I would look to the decoder to answer "What does this P mean" if I encountered one of those chips in the wild. (Though it would also help if "OTP" was defined somewhere in the diagram.)
[/quote]
For the P chips, we decided to exclude them from the part number decoder because there are no new P devices being made. We tried to find a balance between the old and new devices without making the decoder all inclusive and too extensive. Hopefully this decoder can be a useful tool that may be applied to a wide variety of MSP430 parts. Any questions with other part number definitions may be posted to the forum for clarification.
Thank you for reviewing this!
I wholeheartedly agree. I too prefer if a data source tells the whole story, not just the latest version. That's why many people use versioning systems.Peter Bigot said:I don't think the details in the PN decoder should be limited to currently available chips; ideally it will cover the entire product history,
Even it has been a bug/typo that has been removed, I want to knwo it. because maybe I relied on this typo and not, since it is corrected, I need to know that there was a change that may have impact on my code/design.
Or when coding a compiler, you'll need to know which workarounds to implement even for the older silicon. Not just for the latest one.
So it was jsut coincidence, but I was assuming the '09' was referring to the 0,9V minimum operating voltage. Or the 'L09' together.Stephanie Hsu said:We originally defined "0" as the low voltage series
When reading about the L092 first, i thought " why isn't there flash? Nobody will start to develop on this baby if it needs external circuitry and can be developed/debugged on the target board"
My idea was to implement flash - with an internal charge pump. So on boot, flash is operational and the code can be copied to ram, then the charge pump is shut off and flash is deactivated. Reprogrammable, still low power, convenient, and no need fo a high-volume count for the rom versions. And the FLASH version can be 1:1 replaced with a ROM version for mass production.
But there are still available somewhere,. So if someone stubles across it and tries to look it up on the selector, he'll not find it there, maybe asking himself whether this might be a fake chip, a printing error, or whatever.Stephanie Hsu said:For the P chips, we decided to exclude them from the part number decoder because there are no new P devices being made.
Understandable, but IMHO a fact sheet should cover everything. Imagine Windows would silently remove links and files from your desktop or harddisk, just because you didn't click on them for some time. (Yes, it notifies for unused items on the desktop, but even if I agree to remove them, they are collected in a folder on the desktop and not deleted)Stephanie Hsu said:We tried to find a balance between the old and new devices without making the decoder all inclusive and too extensive.
Hi All,
Here is a new part number decoder for your reference:
http://e2e.ti.com/blogs_/b/msp430blog/archive/2013/07/21/msp430-secret-decoder-ring.aspx
I just learned that the latest Windoze version really does this. No notification or assistant that you can cancel. Links are simply vanishing (except, of course, those that Microsoft things you should have on your desktop - even if you don't use them and never intend to use them). Looks like my 1.5 years old doomsday vision has become true.Jens-Michael Gross said:Imagine Windows would silently remove links and files from your desktop or harddisk, just because you didn't click on them for some time.
Thanks for the update.William Cooper said:Here is a new part number decoder for your reference:
One remark: "BT" isn't pre-programmed with Bluetooth. It comes with a BT stack license included (and you need an IAR full license to make use of it), but neither has the requied BT hardware included nor does it have (at least AFAIK) anything pre-programmed (which wouldn't make sense, as you have to reprogram the chip anyway to add any useful application). It's just a re-labeled MSP430F5438A with an undisclosed marker that allows the BT stack library to verify the license.
**Attention** This is a public forum