Part Number: LP-MSPM0C1104
Tool/software:

Hello all,
When I try to flash the example code in MSPM0C 1104 development board then I frequently get this error. Can anyone suggest me the solution to resolve it ? Thank You
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0C1104
Tool/software:

Hello all,
When I try to flash the example code in MSPM0C 1104 development board then I frequently get this error. Can anyone suggest me the solution to resolve it ? Thank You
Can you share your software environment first?
By the way, you are using the launchpad, right?
Yes I am using Launchpad LP-MSPM0C1104.
CCS Version: 12.7.1.00001
MSPM0: sdk_2_00_01_00
If you have any tutorial related to this error please share the link.
I just try to factory reset the board but after connecting the board nothing is shown on output console(like device is ready to attach) So what does it means?
After attach, execute then can be clicked.

After factory reset, the output console will be like below


After attach the board there is no option to select the DSSM drop down function and then to execute.
This may be related to browser. You can try the Chrome.
But anyway, let me attach the document for unlock M0 as another reference.
**Attention** This is a public forum