This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438: finding alternative Safety integrity level (SIL) certified microcontroller

Part Number: MSP430F5438

Tool/software:

hi team,

Previously we are using MSP430FR2476TPT part number as an microcontroller in our project,

Please share the series of Part numbers which are Safety integrity level(SIL2/SIL3) certified MCU which can be replaced by MSP430 series MCU.

  • Hi Hithesh,

    I would recommend below:

    M0L1306QRHBQ1: 32 pin package with AEC-Q100 qulified. And it is FS-QM, which could be used to enable an ASIL-B system.

    MSPM0G3507QPTQ1/MSPM0G3507QPTQ1:48pin QFP package with AEC-Q100 qulified. And it is FS-QM, which could be used to enable an ASIL-B system.

    The above device is RTM and you can check the information in ti.com. 

    We also will support some ASIL-B certificated device with MSPM0L/MSPM0G family, while the information is NDA so you should contact TI regional sales team to check whether you can get details information.

    B.R.

    Sal

  • Hi Hithesh,

    I want to add one additional clarification. The ASIL-B is a automotive safety integrity level, the difference with SIL-2 should be evaluated by end equipment customer.

    B.R.

    Sal

**Attention** This is a public forum