This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3507: MSPM0G3507

Part Number: LP-MSPM0G3507
Other Parts Discussed in Thread: MSPM0G3507, SYSCONFIG

Tool/software:

Hi Experts,

I am new to MSPM0.  I have two question about synchronization with cross trigger in 25.2.7 of TRM.

1. Does timer has multiple cross trigger output?

2. In point 2 of 25.2.7.1, how do I complete this step?

Thanks and Best Regards,

Hook

  • Hi Hook,

    A timer can generate multiple cross trigger outputs by publishing to a split event channel. This can be configured using Sysconfig. On the MSPM0G3507, the split event channels are channel ID 12-15.

    To complete the step mentioned in step 2, you can simply use Sysconfig as well. Open the timer tab in Sysconfig and add one timer instance, then expand the Advanced configuration and Event Configuration tabs. Fill them out to look like mine below. Note that some menus only appear once you have selected to enable the cross trigger. 

    Next, add a second timer instance, and fill it in with the below settings:

    This will give you the configuration you've highlighted in your post.

  • Hi Dylan,

    Thank you for the information you provided. It completely answered my question.

    Best Regards,

    Hook

**Attention** This is a public forum