Part Number: MSP430G2553
Tool/software:
Hi everyone,
I am currently working for a project in which I have three analog inputs on PIN1.1, PIN2.2 & PIN2.4. I want to read all of these PINs with my ADC.
Currently I am doing this with the ADC10 and I am reading the three inputs in sequence. But I don't know how to specifically use the PIN1 and afterwards the PIN2 for the ADC.
Thank you very much for your help.
Yours sincerely,
Timo
#include <msp430.h>
#include <stdint.h>
#define CURRENT BIT1 // Pin 1.1
#define VOLTAGE BIT4 // Pin 2.4
#define TEMPERATURE BIT2 // Pin 2.2
volatile uint16_t current = 0; // Variable to store ADC result
volatile uint16_t voltage = 0; // Variable to store ADC result
volatile uint16_t temperature = 0; // Variable to store ADC result
void start_ADC_conversion();
void main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
ADC10CTL1 = INCH_4 + ADC10SSEL_1; // Channel select A4 + Conversion sequence mode select == Sequence-of-channels + ACLK - clock (no input div)
ADC10CTL0 = SREF_0 + ADC10SHT_2 + ADC10ON + ADC10IE; // REF = VCC & VSS + ADC SampleAndHoldTime 16 x ADC10CLKs + + //
ADC10AE0 |= CURRENT; // These bits enable the PIN 1.1 for analog input
ADC10AE0 |= (VOLTAGE | TEMPERATURE); // These bits enable the PIN 2.2 & 2.4 for analog input
P1SEL |= CURRENT; // ADC input select mode P1.1
P2SEL |= (VOLTAGE | TEMPERATURE); // ADC input select mode P2.2 & 2.4
__bis_SR_register(GIE); // Enable global interrupts
while (1) {
start_ADC_conversion(); // Start an ADC conversion
__delay_cycles(500000); // Delay for a while (for demonstration purposes)
}
}
void start_ADC_conversion() {
ADC10CTL1 = INCH_1; // select channel A1 for ADC
ADC10CTL0 |= ADC10SC + ENC; // ADC10SC == 0 >> no sample start conversation + ENC == EnableConversation
current = ADC10MEM; // saves the ADC measure
while (ADC10CTL1 & ADC10BUSY);
ADC10CTL0 &= ~ENC; // disable conversation
ADC10CTL0 &= ~ADC10IFG; // deletes the ADC-InterruptFlag for the next conversation
ADC10CTL1 = INCH_4; // select channel A4 as input
ADC10CTL0 |= ADC10SC + ENC;
voltage = ADC10MEM; // save ADC measure
while (ADC10CTL1 & ADC10BUSY);
ADC10CTL0 &= ~ENC;
ADC10CTL0 &= ~ADC10IFG; // deletes the ADC-InterruptFlag for the next conversation
ADC10CTL1 = INCH_2; // select channel A2 as input
ADC10CTL0 |= ADC10SC + ENC;
temperature = ADC10MEM; // save ADC measure
while (ADC10CTL1 & ADC10BUSY);
ADC10CTL0 &= ~ENC;
}
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR(void) {
ADC10CTL0 &= ~ADC10IFG; // Clear interrupt flag
__bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit to exit LPM0
}