Other Parts Discussed in Thread: MSP430F5419A, MSP430F5419
We have experienced some difficulties when migrating from msp430f5419 to msp430f5419a in our application
Although the dataseheet states that the A-version should have a lower current consuption than the non A, our application
consumes 50-60uA more when using msp430f5419a. The application is running at 4MHz and spends most of it's time in LPM3-mode.
We have covered the differences listed in TI application report SLAA419B - "Migrating From MSP430F541x/F543x to
MSP430F541xA/F543xA", without having any success lowering the current consumption for the A-device.
To be able to compare the two devices we are running both microcontrollers at PMMCOREV_2 with identical PMM settings
The only difference in software between A and non-A is that REFMSTR is set to '0' in the A-version (the internal reference
is not used in our application)
Clearly we are missing something, but we can't figure out what might be the cause of the increased current consumption
for the A-device
Does anyone have any experience with migrating from msp430f5419 to msp430f5419a ?
Thanks
os