Tool/software:
1) Installed IAR IDE (8.10.3)
2) Imported existing project
3) Triggered Rebuild All
4) Got build error as follows
Fatal Error[e057]: No known CPU specified. The CPU needs to be specified with the -c option. The following processor names are recognized:
5) Here is the device selection based on existing project. Whether this chipset no more available?? If yes how to build this project?