This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-CAPMINI: Firmware binary for CapTivate HID bridge controller (MSP430F5510IRGZT) on EVM430-CAPMINI evaluation Module

Part Number: EVM430-CAPMINI
Other Parts Discussed in Thread: MSP430FR2512,

Tool/software:

I am trying to replicate the Captivate HID bridge (MSP430F5510IRGZT) adaptor part of the EVM430-CAPMINI touch evaluation module. It would be a great help if you could provide me with the firmware binary for the HID bridge controller used on the EVM430-CAPMINI board. The circuit for my HID adaptor is a clone of the HID bridge provided on the EVM430-CAPMINI module, so the production firmware binary used on the EVM430-CAPMINI evaluation module should work fine (See attached Schematic). This bridge module is for interfacing our CapTivate touch circuit based on MSP430FR2512 to the TI's CaptivateDesignCenter Application for calibration and testing.

Thanks,

Thomas

**Attention** This is a public forum