Part Number: MSPBSL
Other Parts Discussed in Thread: MSP-EXP432E401Y
Tool/software:
Hello Team,
I tried to flash the MSP-EXP432E401Y micro-controller with BSL Scripter via ethernet.
Following the procedure mentioned in resource explorer, I have connected one ethernet cable from launchpad to my PC and one LAN cable from company's internal network to my PC.
LOG
MODE E4xx Ethernet MAC=70:ff:76:1c:f2:02 IPClient=192.168.225.67 IPServer=192.168.225.65
Local IP Address is given in the parameter
Local IP Address of Host: 192.168.225.65
Waiting for BOOTP request!
Waiting for BOOTP request!
Waiting for BOOTP request!
Waiting for BOOTP request!
[ERROR_MESSAGE]No BOOTP request received, exit the BSL-Scripter!
I also suspect if it is a firewall related issue, but i'm not supposed to disable the firewall
Can you please tell what should be done to make it work?
Thanks in advance