This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A: Can't disable interrupts.

Part Number: MSP430F5438A


Tool/software:

Hello!

Everything is in the title. Almost.

I would like to temporarily disable interrupts when I enter the ISR and re enable them at the end of the ISR.

In the following example, I use timer B to get a recurrent interrupt. 

The timer itself seems to work, and I have verified with a scope that P10 bits are toggled and that

the period depends on the TBCCR0 value.

Now in order that the program doesn't step on its own feet, I would like to disable interrupts as soon

as it enters into the ISR.

I could verify that:

- The interrupt enable works, be it _EINT(), _enable_interrupts(), bis_SR_register(LPM0+GIE), and possibly

other variants.

- The program doesn't change (i.e. it still works) even if I don't re-enable interrupts at the end of the ISR,

as shown in the following program. I have not re-enabled the interrupts, so it should stop once only in the ISR,

right? But it still works the same (no difference with _EINT() uncommented).

I tried all the variants above with replacing by the relevant function.

Question: is there anything wrong? Is it possible to temporarily disable the interrupts?

int main(void) {
	WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
	P1DIR |= 0x01;                            // P1.0 output
	TBCCTL0 = CCIE;                           // CCR0 interrupt enabled
	TBCCR0 = 50000;
	TBCTL = TBSSEL_2 + MC_2 + TBCLR;          // SMCLK, contmode, clear TBR
//	_enable_interrupts();
	__bis_SR_register(LPM0_bits + GIE);       // Enter LPM0, enable interrupts
//	__no_operation();                         // For debugger
}

// Timer B0 interrupt service routine
#pragma vector=TIMERB0_VECTOR
__interrupt void TIMERB0_ISR(void) {
//	_disable_interrupts();
	__bic_SR_register(LPM0_bits + GIE);
	P1OUT ^= 0x01;                            // Toggle P1.0
	TBCCR0 += 50000;                          // Add Offset to CCR0 [Cont mode]
//	_EINT();
}

By the way: how can I send an image? There is no browse option in the menu -> insert -> image / video file.

If I try to drop a file on the popup window, then I can see the image in my navigator window, but that's not exactly

what I want.

Thanks,

R

**Attention** This is a public forum