Part Number: MSP430FR6972
Tool/software:
Hi
I'm using MSP430FR6972, I want to using the SPI , Uart and I2C, afer the register configuration
example :
SPI2_UCA0
bis.w #UCSWRST,UCA0CTLW0 ;
mov.w #(UCSWRST+UCMSB+UCMST+UCSYNC+UCSSEL1+UCSSEL0),UCA0CTLW0
mov.w #16,UCA0BRW ;* CLOCK DIVISO 2 VA A 500kHz SMCLK èè a 8mHz */
bic.b #(BIT4+BIT3),P4SEL0 ;* disable uart Port 4
bic.b #(BIT0+BIT1+BIT2),P2SEL1
bis.b #(BIT0+BIT1+BIT2),P2SEL0 ;* enable SPI Port 2
bic.w UCSWRST,UCA0CTLW0
SPI2_UCB1
bis.w #UCSWRST,UCB1CTLW0
mov.w #(UCSWRST+UCMSB+UCMST+UCSYNC+UCSSEL1+UCSSEL0),UCB1CTLW0
mov.w #16,UCB1BRW
bic.b #(BIT1+BIT2),P3SEL0 ;* disable I2C on Port 3
bclr.b #(BIT5+BIT6+BIT7),P4SEL0 ;
bclr_b #(BIT5+BIT6+BIT7),P4SEL1 ;* enable spi port 4
bclr.w #UCSWRST,UCB1CTLW0
I have problem with SPI_UCA0, do not have any signal on the output pin whne is set like SPI
if I'm using this port like I/O pin work properly
, the SPI_UCB1 work properly without any problem,
for the SPI_UCA0 there is some bit in the hide Register to enable the SPI ? I have try to check every where
but did't find anythings
Luigi
have problem only with port 2, there is some special bit on sonme hide register ?