Tool/software:
Hello
for an anemometer, we first wanted to measure the wind speed via an ultrasonic sensor. (Single Ton) We use the following sensor: CUSP-TR12-010-1150-WC. The values have been set for the time being, but with Volume Flow Rate there is no exact data such as - 47 liters in 10 minutes. The fan runs at 29.2 m³/h at maximum speed. Maybe you can help me with the configuration a bit. Attached are the following pictures: