Tool/software:
Hello TI experts!
Please kindly to give us some advice,
Ask 3 questions:
1) In the USS tool, on the interface of "Calibration-VFR flow-temperature", the actual data such as meter ID, flow ID, and TEMP ID under MEASUREMEMTS are stored in which file , and the file name of the measurement data is stored. (We are considering batch data calibration, and we need to use this file to speed up the calibration)
2) How to do bubble detection in water, what are the suggestions to achieve bubble detection?
3)Piecewise fit calibration, at the junction, there will be mutations, and there is any way to eliminate or reduce these mutations