Part Number: EVM430-FR6047
Tool/software:
TI experts, please kindly help us point us out:
1) We use DN20 pipe, we need to achieve R400, the minimum flow point is 0.016 m3/h,
using segmented fitting calibration, it is recommended to divide how many RANGE ?each section 5~10 points.
2) Each water meter, as long as it is calibrated once, a calibration table can be generated,
or it needs to be calibrated many times repeatedly to produce stable and accurate calibration table
3) In the calibration of USS, why does the VFR flow need to set the Error Threshold, but not the VRF flow+ Temperature?
4) In the USS tool, there is no place to enter RANGE in VRF flow+ Temperature mode, in fact the RANGE is define by us , we manually segment the data and input it into measurements table,
only no RANGE prompt, right?