This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5329: Using UART at 1M baud rate

Part Number: MSP430F5329

Tool/software:

Hello,

I am trying to use UART at 1M baud rate with F5329 which is beyond the highest baud rate in the "Commonly Used Baud Rates" table in the datasheet. My BRCLK is 12MHz. I found it possible with right prescaler and modulator settings and got it running at 1M. 

However, I am experiencing time out issues in the communication at not only 1M but also at all the baud rates beyond 460800. My question is, why is the table capped at 460800? Is there any reason or data behind this table? And most importantly, is it possible to use 1M baud rate on F5329? Thank you!

Best Regards,
Cheng

**Attention** This is a public forum