This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F47187: Clock initialization for 8Mhz Crystal

Part Number: MSP430F47187


Tool/software:

As i understood its a low-power micro controller which works on 32.768 kHz,

Can i configure the Clock initialization using 8MHz.

What will be the DCO / MCLK / SMCLK

Also ADC SD16A to be of 1ms interrupt.

Is it possible to do the same, 

**Attention** This is a public forum