This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969-SP: Using the MSP-FET, but want to run UART at 230K

Part Number: MSP430FR5969-SP
Other Parts Discussed in Thread: MSP-FET

Tool/software:

I see that the maximum baud rate for the MSP-FET is at 115200 baud. For my design, I want to run the UART at a faster rate - 230,400.

I am wondering what my options are.

Is there another tool that would support this for testing? I have the MSP FET connected to a custom board that I designed.

Thanks!

**Attention** This is a public forum