This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5638: GPIO 16 bit data transfer between two MCU's ports

Part Number: MSP430F5638

Tool/software:

Custom SBC with one MSP430F5638 and one MSP432P401R MCU's. Each MCU is running on a 2 second period, sleeping most of the time, then repeats endlessly.

430 PA (P1+P2) connected to 432 PB (P3+P4)

I can send a single variable from one to the other via PxIN and PxOUT, but want to send an array of ints in every 2 second period. Neither MCU has access to the others memory space. This seemed like a good idea when I designed the board, but am not sure how to proceed. Seems like what I might need is: dueling ISR's on each end, sending a single array element, until end of array. Did not find any TI code examples for this type of transfer.

Any experience with this or suggestions?

**Attention** This is a public forum