This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2453: 2-Wire programming not working with all MSP-FET Programmers

Part Number: MSP430G2453
Other Parts Discussed in Thread: MSP-FET

Tool/software:

Hello,

I have a problem that should not exist - related to 2-wire JTAG programming

I have x2 MSP-FET430UIF programmers - One works in 2-wire mode - one does not.

So I ordered x2 new MSP-FET Flash emulation tools - and neither one works. (read on)

Referencing the slau278ah.pdf page 22 - figure 2-2 -  I have a 33K verses a 47K pullup to 3.3 Volts - but that is the only difference.

Additional info - I jumpered out R2 and disconnected pin 8 (TEST/VPP) - and now it works with the new MSP-FET pods.

Can someone explain this behavior ?

.js.

**Attention** This is a public forum