Tool/software:
Hello All,
We are Designing Water meter product for our client. We have selected mspfr6043 for measuring the flow rate .
We referred uss library water demo for the same chip and try to analysis the working of application.
Based on the application design. We have some mandatory requirements as below based on requirement of client.
1. Water Leakage Detection
2. Backflow detection
3. Empty pipe detection
4. Broken Pipe Detection.
5. Air bubble Detection
Is there any method ,ref code or Document reference which can be used to fulfill above features?
Any help will greatly appreciated.
Thanks & Regards,
Amit Pramamik