Part Number: MSP430F6775A
Tool/software:
Hi,
I would like to ask whether the configuration in the LCDC module, which contains the resetting bit REFCTL0 &= ~REFMSTR, has any effect when REFON is set to 0. Is it correct to set it this way? In the example for msp430f677xA-lcdc-01.c, it is used, but the documentation states, “Devices with ADC10_A do not support this mode. The REFMSTR bit must not be cleared.” I am also sending the screen from the documentation for REFCTL0 and the code example. I just want to be sure which configuration is correct because, according to the documentation, it should not be set to zero since the msp430f6775a device contains ADC10_A. Am I wrong?