Tool/software:
I am using the EMDC software to generate code for i2041. The configuration has one voltage channel and one current channel with CT.
Unfortunately, we could not get the HID to work with 5529LP. The green LED never blinks on 5529LP even after programming the TXT file many times. We can not long put more effort on that as we need to get the rest of the system working.
So, we are going through the UART protocol on i2041 and interface to a host MCU. Since the EMDC GUI is not present, we see values around 6000 decimal in gEmSWResult.phaseResults[phaseIdx].VRMS variable. The input voltage is 230V AC at 50Hz with voltage divider with 1.8k and 2M resistor.
Question:
1. Is the EMDC GUI converting the ADC sample values to the actual values - as in, 6000/32767 * 1.2 * 2000 / 1.8 = 244 Vrms? Here, 1.2 is Vref.
2. If the EMDC is not converting the ADC values to the actual values, then is this a part of the "calibration" commands where the voltage divider, and current shunt related scaling factors are programmed into i2041?
3. Whether #1 or #2, it seems we have to do the same on the host MCU in our system - right? Is there a way to do this math in the i2041 metrology MCU itself?
Please advise. Thanks.