This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR6989: Boards won't run project

Part Number: MSP-EXP430FR6989

Tool/software:

Sorry in advance for any confusion I may cause. I have used these boards for a while now but just recently actually started to dig a little deeper. I have purchased about 7 of these boards and i wanna say 4 of them do not work and they have the same issue. I have a project that I use for work. It is designed to read and write to a device's EEPROM. I've used this project for a long time, so I am 100% that the code itself is not the issue. The boards that do not work will power on, the code will debug and run properly but do not read or write to the EEPROM. I use the serial COM port to monitor the data Read/Write and it does not do either. The board is recognized on the COM as connected so the issue is not with that either.  

**Attention** This is a public forum