This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5989: Interference problem

Part Number: MSP430FR5989
Other Parts Discussed in Thread: CC1120,

Tool/software:

We need to design a new system, which includes 434Mhz narrowband (CC1120) and mesh network based on 868MHz and 27dB PA (CC110x+FEM). They work on their own antenna (wired or PCB), but asynchronous. Same to you. 434Mhz doesn't know 868Mhz, and vice versa: there is a SOM control module based on Linux, but the module only receives/sends data to SOM, and the module itself organizes the RF part. I'm not sure: what will happen/what will happen and how to avoid it? For example, if 434Mhz sends something and 868MHz only receives something: won't 434Mhz harmonics damage this process? This may be a special application. 434 and 868 can coexist. Can you ask your fae for help?

**Attention** This is a public forum